Diodes|Basic
PIN Diodes
table of contents
Structure and Features
| Structure | Symbol | Applications・Characteristics |
|---|---|---|
![]() |
|
A high resistivity I-type semiconductor is utilized to provide significantly lower diode capacitance (Ct). As a result, PIN diodes act as a variable resistor with forward bias, and behave as a capacitor with reverse bias. High frequency characteristics (low capacitance ensures minimal effect of signal lines) make them suitable for use as variable resistor elements in a wide variety of applications, including attenuators, high-frequency signal switching (i.e. mobile phones requiring an antenna), and AGC circuits.
| Forward Voltage | Reverse Voltage |
|---|---|
![]() |
|
| Variable resistance with forward bias |
Capacitor with reverse biase |
What is the Diode Capacitance (Ct)
The amount of accumulated charge internally when supplying a reverse bias is called the diode capacitance (Ct). An electrically neutral depletion layer is formed by filling the intrinsic layer – created between P and N layers – with charge carriers (holes and electrons). The depletion layer acts as a parasitic capacitor, with a capacitance proportional to the PN junction area and inversely proportional to the distance d. The distance is determined by the concentration of the P and N layers. Supplying a voltage to the diode will increase the depletion layer and decrease Ct.The required Ct will vary depending on the application.
[When supplying a reverse voltage]

Key Points
- The wider the depletion layer (and greater the distance) the lower the capacitance Ct.
【Download Documents】 Transistors & Diodes Basics and Selection
In this handbook, although there are so many types of power devices using Si semiconductors, the basic points are explained, focusing mainly on diodes and transistors for power supply applications. It also introduces the procedure and decision method for transistor selection when designing circuits, as well as application examples that utilize each characteristic and feature.
Diodes
Basic
-
Diode Articles
- What is a pn junction?
- What Is a Diode? How It Works, Types, and Applications
- Rectifier Diodes
- Switching Diode
- Schottky Diode (Schottky Barrier Diode)
- Zener Diode
- TVS Diodes
- PIN Diodes
- Diode Types and Characteristics: Static and Dynamic Characteristics, Current, Voltage, and Reverse Recovery Time
- Comparing Rectifier, Switching, Schottky, and Fast Recovery Diodes
- Schottky Diode Characteristics and Thermal Runaway
- Fast Recovery Diode (FRD) Characteristics
Evaluation