Motor|Basic
Driving of Brushed DC Motors Using BTL Amplifier Circuits: Linear Current Driving
2022.07.06
Points of this article
・An example of a linear current driver for brushed DC motors applies a BTL amplifier to motor driving.
・A BTL amplifier can be used for brushed DC motor driving by either voltage driving or current driving.
In succession to the previous article, ”Driving of Brushed DC Motors Using BTL Amplifier Circuits: Linear Voltage Driving”, here the use of a BTL amplifier for linear current driving is explained.
Driving of Brushed DC Motors Using BTL Amplifier Circuits: Linear Current Driving
The following is a BTL amp circuit that performs linear current driving of a brushed DC motor.

A resistor Rs for current detection is inserted between the motor and the output OUT1, so that the current flowing to the motor is detected as a voltage, which is used for negative feedback to the input-stage amplifier. Through this feedback, the input-stage inverting amplifier performs feedback control of the output voltages of the two output-stage power amplifiers. The output-stage amplifiers are differential amps; the output M0 of the input-stage amp is received by the inverting input of the OUT1 amp, and is received by the non-inverting input of the OUT2 amp, so that OUT2 is opposite in phase from OUT1. Overall, the circuit can be considered to be a single-ended input, differential output (normal phase/inverted phase) amplifier.
The relationship between the input voltage and the output current is as follows. The output current (motor driving current) is fed back to the inverting terminal of the input-stage inverting amplifier as the output Vso of the differential amplifier that detects and amplifies the voltage difference (voltage drop) across the current detection resistor Rs. Vso can be found using the equation below. As is clear from the connections of Rs, Vso is a voltage that is inverted with respect to the current direction.
Vso=-Rs・Io・(R6/R5)+Vref
Further, if the voltage applied to the input terminal IN1 is VIN1, then upon setting the input-stage amp gain to be infinitely high, the voltage at the inverting input terminal becomes Vref.
From the principle of operation of an inverting amplifier, control is executed such that the sum of the currents at the inverting input terminal of the input-stage inverting amplifier is 0 A. That is, the following equation obtains.
which, modified, becomes ![]()
Rs(R6/R5) is a fixed value, and so the output current Io can be set to a desired value by adjusting VIN1.
Current driving has the feature that, when the current is less than the current setting, the motor is driven at maximum voltage, so that the time until the current setting is reached is short, and the motor response is fast. Moreover, in this article an example of linear driving was presented, but similarly for PWM output, current driving is possible by detecting the current and executing negative-feedback control.
【Download Documents】 Basics of Brushed DC Motors and Drive Methods
Brushed DC motors are the most versatile motors and are used in a great many applications. This handbook provides the basics of brushed DC motors, explaining their construction, principle of operation, characteristics, and driving methods.
Motor
Basic
-
Brushed DC Motor
- Construction of Brushed Motors
- Principle of Rotation
- Power Generation Principle
- Short Braking
- Characteristics of Brushed DC Motors
- Driving Brushed DC Motors with an H-Bridge:Principles
- Driving Brushed DC Motors with an H-Bridge:Switching Output States
- Driving Brushed DC Motors with an H-Bridge:High-Side Voltage Linear Control
- Driving of Brushed DC Motors Using BTL Amplifier Circuits: Linear Voltage Driving
- Driving of Brushed DC Motors Using BTL Amplifier Circuits: Linear Current Driving
- Driving Brushed DC Motors Using PWM Output: Principles of PWM Driving
- Driving Brushed DC Motors Using PWM Output: Current Regeneration Methods in PWM Driving
- Driving Brushed DC Motors Using PWM Output: Losses and Points to be Noted
- Driving Brushed DC Motors Using PWM Output: PWM Driving with an H-Bridge Circuit
- Driving Brushed DC Motors Using PWM Output: H Bridge Constant-Current Driving
- Driving Brushed DC Motors Using PWM Output: Driving in the Form of BTL Amplifier Input
- Single-Switch Circuit Driving and Half-Bridge Circuit Driving
- Driving Circuits for Brushed DC Motors – Summary
-
Stepping Motors
- Structure of Stepping Motors
- Basic Operating Principles of Stepping Motors
- Stepping Motors: Microstep Operation Principles
- Basic Characteristics of Stepping Motors
- Structure and Operating Principles of Hybrid Type Stepping Motors
- Stepping Motor Driving: Bipolar Connections and Unipolar Connections
- Driving 2-Phase Bipolar Stepping Motors: Part 1
- Driving 2-Phase Bipolar Stepping Motors: Part 2
- Driving 2-Phase Unipolar Stepping Motors
- Stepping Motors – Summary
-
3-Phase Brushless Motors
- Structure of 3-Phase Full-Wave Brushless Motors
- Principles of Rotation of 3-Phase Full-Wave Brushless Motors
- Position Detection in 3-Phase Full-Wave Brushless Motors
- Driving 3-Phase Full-Wave Brushless Motors: 120° Commutation Linear-Current Driving with Sensors
- Driving 3-Phase Full-Wave Brushless Motors: Sinusoidal Commutation PWM Driving with Sensors
- Driving 3-Phase Full-Wave Brushless Motors: Advance Angle Control
- Driving 3-Phase Full-Wave Brushless Motors: Maximization of Motor-Applied Voltage
- Driving 3-Phase Full-Wave Brushless Motors: Sensorless 120° Commutation Driving
- Methods of Sensorless 120° Commutation Driving Startup 1: Startup on Detection of Induced Voltage from Synchronous Operation
- Methods of Sensorless 120° Commutation Driving Startup 2: Startup on Detection of Permanent Magnet Stopped Position
- Features and Applications of 3-Phase Full-Wave Brushless Motors ーSummaryー
- What is a Motor?