AC-DC|Basic

Certifications and Regulations

2015.12.06

Points of this article

・Corresponding to various regulations and certification requirements, methodical research and a schedule for compliance must be developed.

・One must be prepared to face the required costs, in time and money, to clear the hurdles of tests and reviews.

Power supply units are subject to a number of regulations and bear several certifications, as the familiar Energy Star logo, pertaining to efficiency and standby power consumption, attests. In the area of safety, the PSE certification is required on AC adapters and power supplies. In terms of noise reduction, there are many cases in which EMI and EMC compliance is required. These requirements are a diverse set, some being applicable across the world and others limited to a specific country or region. Any product offered globally needs to comply with the regulations applicable in the respective countries. Furthermore, it should be borne in mind that acquiring such certifications requires tests, with attendant time, expenses, and a considerable amount of work.

Figure 39

An important component of a design process is a firm grasp, at the outset, of what certifications are required and what regulations must be complied with. If such requirements are added as an after-thought, one may end up revamping the whole design or, even if the product development has been finished, one may be stuck in a situation where the product cannot be shipped because the requisite testes have not been completed, with veritable disastrous consequences.

【Download Documents】 Basics of AC-DC Converter and Design Procedures

A hand book for beginners to AC-DC converter design, covering the basics of AC-DC conversion and various conversion methods, as well as the procedures and issues involved in designing an AC-DC converter.

    AC-DC

    Basic

    Design

    Evaluation

    Product Information

    FAQ