Electrical Circuit Design|Basic
Kirchhoff’s Circuit Laws
2025.08.06
table of contents
- ・Kirchhoff's Current Law and Voltage Law
- ・The Role of Kirchhoff's Laws in Voltage and Current Measurements
- ・Simultaneous Equations in Circuit Analysis
- ・Ohm’s Law and Kirchhoff’s Laws
- ・Kirchhoff’s Law Practical Examples and Calculation Method
- ・Potential Difference and Electromotive Force: Relation to Kirchhoff’s Laws
Kirchhoff’s laws are the most fundamental principles used in the analysis of electrical circuits. Applying these laws enables efficient circuit analysis based on understanding the distribution of currents and voltages in complex circuits. This article presents the concepts of Kirchhoff’s laws, explains their application to real circuits, and describes their relationship to Ohm’s Law. Learn Kirchhoff’s laws, essential for studying electric circuits, and use them as a powerful analysis tool.
Kirchhoff’s Current Law and Voltage Law
Kirchhoff’s laws consist of two laws: the first is Kirchhoff’s Current Law (KCL), and the second is Kirchhoff’s Voltage Law (KVL). Each law is explained below.
Kirchhoff’s Current Law (KCL)
Kirchhoff’s Current Law is the principle that the sum of the currents flowing into a contact (node) equals the sum of the currents flowing out of that contact. This can be expressed in mathematical terms as follows:
\(\sum I_{in}=\sum I_{out}\)
The law implies that charge cannot accumulate at any circuit node.

Kirchhoff’s Voltage Law (KVL)
Kirchhoff’s Voltage Law (KVL) states that the sum of the voltages around any closed loop in a circuit equals zero. It is expressed as follows:
\(\sum{V=0}\)
This law is based on the law of energy conservation, which means that the sum of the voltage drops and the electromotive forces will remain in equilibrium.

Closed Circuit and Open Circuit
This section discusses closed circuits, as referred to in Kirchhoff’s voltage law. Understanding the concept of closed and open circuits is very important in circuit analysis; when applying Kirchhoff’s voltage law, it is necessary to identify whether a circuit is closed.
In addition, the term closed loop refers to any continuous conductive path used to apply KVL, whereas a closed circuit generally implies a loop that also conducts current. KVL applies to the former regardless of whether current actually flows.

Closed Circuit
A closed circuit is one in which the current has a complete path back to the power source through a series of conductors. In other words, it starts at the power source, passes through electrical elements such as resistors, capacitors, and inductors, and returns to the power source again. In a closed circuit, the current flows continuously, and voltage drops are distributed among the circuit’s elements.
The concept of closed circuits is central to the design and analysis of electrical circuits. To understand and predict the exact behavior of electrical elements, it is necessary to understand the relationship between current and voltage within a closed circuit composed of these elements. Closed circuits also play an essential role in evaluating circuit performance and diagnosing problems.
Open Circuit
An open circuit has no complete path for current to flow because of an interruption midway in a conductor. This is caused by some disconnection, such as a turned-off switch or a physical break in the circuit.
Kirchhoff’s Voltage Law (KVL) still holds for any closed path, even if that path contains an open branch through which no current flows. In an open circuit the loop current is zero, but the algebraic sum of the potential rises and drops around a closed path remains zero. It is an essential principle when a circuit is not functioning correctly or when open circuits are incorporated during the design phase. In failure analysis and troubleshooting, open circuits are likely causes of problems and play an essential role in the diagnostic process.
The Role of Kirchhoff’s Laws in Voltage and Current Measurements
Voltage Measurements and the Application of Kirchhoff’s Voltage Law
Voltage measurement is essential for understanding electrical circuits, and Kirchhoff’s Voltage Law plays a central role in this process.
Basics of Voltage Measurement
Voltage measurement determines the potential difference between two points in a circuit, typically using a voltmeter connected in parallel between the two points to be measured.

Application of Kirchhoff’s Voltage Law (KVL)
Kirchhoff’s voltage law makes it possible to measure and calculate the voltage across any loop in a circuit. In other words, once a few branch voltages are measured with a voltmeter, KVL allows the remaining unknown voltages in the same loop to be calculated algebraically.
Importance of Current Measurement and Circuit Analysis
Current measurement and circuit analysis are essential for evaluating circuit performance and safety.
Current Measurement Method
Current measurement measures the current flowing through a part of the circuit. It is done using an ammeter connected in series at the point to be measured.

Kirchhoff’s Current Law (KCL) and Circuit Analysis
Kirchhoff’s current Law makes it possible to analyze the distribution of currents at any point in a circuit and evaluate the circuit’s functionality.
Simultaneous Equations in Circuit Analysis
Simultaneous Equations Using Kirchhoff’s Law
When performing circuit analysis using Kirchhoff’s laws, it is essential to set up simultaneous equations.
The analysis proceeds in four steps:
-
Identify the circuit: identify all nodes (contacts) and loops (closed circuits).
-
Apply Kirchhoff’s current Law: at each node, set an equation indicating that the sum of the incoming currents equals the sum of the outgoing currents.
\(\sum I_{in}=\sum I_{out}\)
-
Apply Kirchhoff’s voltage law: For each loop, set an equation indicating the zero-sum of the loop’s voltages.
\(\sum{V=0}\)
-
Solve the equations: Solve the resulting equations to find the unknown currents and voltages.
Application to Real Circuits
Consider the series circuit shown in Figure.
Suppose resistors of different resistance values are connected in a simple series circuit. To find the voltage across each resistor in the circuit, we follow the steps:
-
KVL: Set the equation for the KVL for the entire circuit.
\(V_{source}=V_1+V_2+\ldots+V_n\)
Vsource is the voltage of the power source, and V1, V2,…, and Vn are the voltages across the respective resistors.
-
Ohm’s Law: Use Ohm’s Law to find the voltage across each resistor:
\(V_i=I\times R_i\)
Where I is the current in the circuit, and Ri is the resistance of the resistor.
-
Solve the Equations: Find the voltage across each resistor.
Ohm’s Law and Kirchhoff’s Laws
Two Complementary Laws
Kirchhoff’s voltage law and Ohm’s Law complement each other in circuit analysis.
What is Ohm’s Law?
Ohm’s Law expresses the relationship between voltage (V) and current (I) in a conductor and is expressed by:
\(V=I×R\)
where R is resistance.
Combined with Kirchhoff’s Voltage Law
By combining Kirchhoff’s voltage law and Ohm’s Law, it is possible to analyze more complex relationships between voltage and current in a circuit. It helps determine unknown voltages and currents in a circuit.
Applying to DC and AC Circuits
The application of these two laws differs for direct current (DC) and alternating current (AC) circuits.
Application to DC Circuits
In a DC circuit, current flows in a constant direction, and voltage is also continuous. In such a DC circuit, Ohm’s Law and Kirchhoff’s voltage law can be used to calculate the voltage and current for each element in the circuit.
Application to AC Circuits
In AC circuits, voltages and currents vary with time. Therefore, when applying Ohm’s Law and Kirchhoff’s voltage law, it is necessary to consider AC characteristics such as phase difference and frequency.
Kirchhoff’s Law Practical Examples and Calculation Method
Step by Step with Examples
Consider a simple circuit in which resistors R1, R2, and R3 are connected in series, and a power supply VS is provided for the circuit. Let us find the voltage drop across each resistor.

1. Circuit Analysis:
First, identify each element of the circuit.
- ・ Power Supply (VS)
- ・ Resistor 1 (R1)
- ・ Resistor 2 (R2)
- ・ Resistor 3 (R3)
2. Kirchhoff’s Voltage Law (KVL):
The sum of the voltages around a closed loop in a circuit is zero.
\(V_S=V_1+V_2+V_3\)
where VS is the voltage of the power source, and V1, V2, and V3 are the voltages across R1, R2, and R3, respectively.
3. Ohm’s Law:
Ohm’s Law is applied to each resistor.
\(V_i=I\times R_i\)
4. Calculation:
Calculate the voltage across each resistor using the power supply voltage and each resistor value.
According to Ohm’s Law, the voltage across each resistor can be calculated as:
\(V_1=I×R_1\)
\(V_2=I×R_2\)
\(V_3=I×R_3\)
where I is the current flowing through the circuit.
5. Substitution for Kirchhoff’s Law
Substitute these into Kirchhoff’s Voltage Law equation:
\(V_S=I×R_1+I×R_2+I×R_3\)
This equation shows that the voltage drop in a series circuit equals the voltage of the power supply.
Applying Kirchhoff’s Laws to a Complex Circuit
Consider the following circuit containing multiple power supplies and resistors.

The circuit is connected as follows:
- ・VS1 and R1 are connected in series.
- ・R2 is connected in parallel with this combination.
- ・This parallel circuit is connected in series with R3.
- ・Finally, VS2 is connected after R3.
The following equations hold:
-
・Loop 1 (left mesh VS1 → R1 → R2):
\(V_{S1}-I_1×R_1-I_2×R_2=0\)
-
・Loop 2 (outer mesh VS1 → R1 →R3 → VS2):
\(V_{S1}-I_1×R_1-I_3×R_3-V_{S2}=0\)
-
・Loop 3 (right mesh VS2 → R2 → R3, clockwise, starting at the negative terminal of VS2):
\(V_{S2}-I_2×R_2-I_3×R_3=0\)
I1, I2 and I3 currents flow through the respective circuit parts.
Analyze according to the following steps:
- Identify circuit elements: Identify all power sources, resistors, nodes, and closed loops.
- Apply Kirchhoff’s laws: KVL to each closed loop and KCL to each node.
- Simplification: Set up simultaneous equations.
- Calculation: Solve the equations to obtain the unknown currents and voltages.
Potential Difference and Electromotive Force: Relation to Kirchhoff’s Laws
What is Potential Difference?
Potential difference is a fundamental concept in electrical circuits closely related to Kirchhoff’s Laws. Potential difference is the difference in electric potential (level of electrical energy) between two points. The potential difference represents the amount of work required for an electric charge to move from one point to another and is expressed in volts (V) with the following equation.
\(V=W/Q\)
V is the potential difference, W is the work, and Q is the charge.
Relationship between Potential Difference and Kirchhoff’s Laws
The concept of potential difference is essential when applying Kirchhoff’s laws to understand voltage distribution in a circuit. For example, Kirchhoff’s voltage law can be used to find the potential difference across each section in a circuit with multiple voltage sources and resistors. This allows us to determine exactly how the potential difference between the power supplies will be distributed in the circuit.
Electromotive Force and Kirchhoff’s Laws
Electromotive force (EMF) is the potential difference produced by a power source. It is essential to understand EMF in conjunction with Kirchhoff’s laws.
Definition of EMF
EMF is the potential difference created by the energy provided to a circuit by a power source, such as a battery or generator. In other words, it is the energy, expressed in volts (V), that a power supply provides to a circuit. EMF is created by the movement of electric charge due to the electric field produced by the power source.
Relationship to Kirchhoff’s Voltage Law
Kirchhoff’s voltage law states that the sum of the voltages in a closed circuit is zero. The “the sum of the voltages is zero” part of this Law can be rewritten as “the sum of the electromotive forces is equal to the sum of the voltage drops”. This means that the voltage drops, which constitute the energy consumed by the loads in each part of the circuit, are in balance with the electromotive forces due to the power supply. This allows us to understand how the energy supplied by the power sources interacts with the energy consumed by the elements in the circuit, and this knowledge can be used in the design, analysis, and troubleshooting of electrical circuits.
【Download Documents】 DC Circuit Fundamentals
This handbook summarizes the fundamental laws and circuit analysis methods of DC circuits covered in each article. It outlines derivations and circuit behavior, highlighting essential ideas for circuit design.
Electrical Circuit Design
Basic
- Soldering Techniques and Solder Types
- Seven Tools for Soldering
- Seven Techniques for Printed Circuit Board Reworking
-
AC Circuits Fundamentals: Article Guide
- AC Circuits: Alternating Current, Waveforms, and Formulas
- Complex Numbers in AC Circuit
- Fundamentals of Capacitive Circuits: Understanding Series and Parallel Capacitor Connections
- Electrical Reactance
- What is Impedance? AC Circuit Analysis and Design
- Impedance Measurement: How to Choose Methods and Improve Accuracy
- Impedance Matching: Why It Matters for Power Transfer and Signal Reflections
- Resonant Circuits: Resonant Frequency and Q Factor
- RLC Circuit: Series and Parallel, Applied circuits
- What is AC Power? Active Power, Reactive Power, Apparent Power
- Power Factor: Calculation and Efficiency Improvement
- What is PFC?
- Boundary Current Mode (BCM) PFC: Examples of Efficiency Improvement Using Diodes
- Continuous Current Mode (CCM) PFC: Examples of Efficiency Improvement Using Diode
- LED Illumination Circuits:Example of Efficiency Improvement and Noise Reduction Using MOSFETs
- PFC Circuits for Air Conditioners:Example of Efficiency Improvement Using MOSFETs and Diodes
-
DC Circuits Fundamentals: Article Guide
- Electric Current and Voltage in DC Circuits
- Ohm’s Law: Voltage, Current, and Resistance
- Kirchhoff’s Circuit Laws
- What Is Mesh Analysis (Mesh Current Method)?
- What Is Nodal Analysis (Nodal Voltage Analysis)?
- Thevenin’s Theorem: DC Circuit Analysis
- Norton’s Theorem: Equivalent Circuit Analysis
- What Is the Superposition Theorem?
- What Is the Δ–Y Transformation (Y–Δ Transformation)?
- Voltage Divider Circuit
- Current Divider and the Current Divider Rule