Engineer Column

Five Engineers Talk About New Medium-Power Device Products: Part 1 Development of Bipolar Transistors for Gate Driving in Inverter Circuits for xEVs

2021.06.09

Hello, everyone! My name is Tanaka, and I’m in charge of the development of new bipolar transistor products at ROHM.

This is the first of a five-article column in which new power transistor and power diode products are explained firsthand by the engineers tasked with their respective development. These are intended as articles from the engineer’s point of view, in contrast with new product press releases and the like. I hope you find them interesting.

“Bipolar transistors”…hearing this term again may be cause for brief rumination; but as you are aware, they are the most basic of electronic components. Bipolar transistors are one type of transistor, and in general are often simply referred to as “transistors”.

Bipolar transistors are semiconductor elements in which N-type and P-type semiconductors are joined. They can have a P-N-P or an N-P-N structure. They operate using both holes and electrons, that is, using both polarities, and so are called “bipolar”. In general, they have three terminals, called the collector, the base, and the emitter, and they are used for current amplification and as switches to turn circuits on and off.

I’ll note in passing that there exist unipolar transistors, which are contrasted with bipolar transistors. This is not a term that one hears very often these days, but this device is equivalent to a field effect transistor (FET). Well, let’s leave the background knowledge at that and move on to the main subject.

Bipolar transistors, as relatively inexpensive devices used in diverse applications, had been the mainstream of transistor products; but demands for reduced energy consumption in recent years have led to emphasis on higher efficiency, so that in many cases MOSFETs and IGBTs are used instead. However, there are also numerous cases in which bipolar transistor use dominates. We recently developed new bipolar transistors for use in such applications.

The newly developed devices are the 2SAR642PHZG(PNP type) and the 2SCR642PHZG(NPN type), which guarantee a large collector current (pulse) ICPfor gate driving in inverter circuits and the like.

In recent years, electrification of vehicles is accelerating, spurred by environmental problems and fuel issues. Demand for hybrid vehicles and electric cars to replace conventional gasoline-powered cars is increasing, and various pieces of equipment that had not existed in gasoline-fueled cars are being installed.

In particular, high-voltage batteries are mounted in these vehicles, and so there has been increasing demand for high-voltage switching devices for use in battery control. Gate driver ICs are necessary to drive such high-voltage switching devices, but the device operating conditions vary widely depending on the equipment and the intentions of the developers.

Hence in order to enhance the versatility of gate driver ICs, it is increasingly common to provide a bipolar transistor buffer between a gate driver IC and a high-voltage switching device.

As an example, below is shown an inverter circuit configured using a gate driver IC, a switching device (MOSFET or IGBT), and bipolar transistors.

In this circuit example, in order to drive the switching element, a gate driver is needed that can adequately drive the gate capacitance of the switching element in a short length of time. If the driving capability of the gate driver IC is insufficient to drive the switching element being used, it is possible to employ bipolar transistors as a buffer to remedy the problem.

The current capacity of switching elements in the inverter circuits that are increasingly in demand for use in xEV is trending upwards, and bipolar transistors with high current driving capabilities for use in buffers are being sought. For these reasons, our newly developed 2SAR642PHZG and 2SCR642PHZG products feature specifications that reflect these market needs, and guarantee a collector current (pulse) ICP of 10 A in 1 ms. The major product specifications are shown below.

Henceforth we will continue to develop new bipolar transistor products tailored to promising applications and markets. Please watch for further announcements.

【Download Documents】 Silicon Power Devices Application Examples Utilizing the Merits

ROHM’s seminar materials provided at the seminar venue. Silicon base power devices continue its evolution for the market demands of product power saving and efficiency enhancing. Basic knowledge to selection methods for diodes and MOSFETs, the latest device properties, and application examples are described.

    Engineer Column