Learn Know-how

Estimation of Heat Dissipation Area in Surface Mounting and Points to be Noted

2023.01.25

Points of this article

・When heat-generating ICs are mounted close together, thermal interference occurs, inducing rises in temperature.

・The required θJA is found from the allowed maximum TJ, and the resulting necessary heat dissipation area is estimated.

Up to this point, methods for estimating TJ using thermal resistance and thermal characterization parameters have been explained. In this article, a method is described for estimating the heat dissipation area in surface mounting in order to ensure that TJmax is obeyed, and important points relating to the thermal consequences of component layout are explained.

Component Layout and Thermal Interference

Demands for miniaturization in recent years have led to the need for circuit boards that are as small as possible, and component mounting densities are trending upwards. However, components that emit heat, which in this case are ICs, require use of the mounting board for heat dissipation, and to this end a certain area is needed. If this board area is not secured, thermal resistance is higher and heat generation becomes excessive. If heat-generating ICs are mounted in close proximity, interference by their generated heat may cause increases in temperature.

The figures below illustrate heat dissipation paths of a surface-mounted IC, and heat dissipation when heat-generating ICs are in close proximity.

Heat generated by an IC is conducted laterally (over a board area) and vertically (through the board thickness) and is dissipated. However, when ICs are densely mounted, there is mutual interference by heat dissipation in lateral directions in particular–the heat has nowhere to go. Hence temperature increases result.

Estimating the Board Area Needed for Heat Dissipation

In order to ensure that a surface-mounted IC can have a thermal resistance that remains within the TJmax limit, a corresponding heat dissipation area is necessary. In addition, it is also important to ensure that thermal interference does not occur. The diagram below illustrates the interval needed so that there is no thermal interference. After ensuring that this minimum condition is satisfied, the required heat dissipation area is estimated using a graph of the relationship between θJA and the copper foil area.

As the diagram indicates, the minimum interval is set such that there is no interference between straight lines inclined 45° from the edges of ICs to the board surface. Next, the required θJA for the conditions of use is determined.

Conditions example: IC power consumption=1 W, maximum ambient temperature TA(HT)=85°C, maximum allowed TJ=140°C

From the graph on the right, we see that in order to set θJA to 55°C/W, a copper foil area of at least 500 mm2 is necessary.

In this way, IC intervals that avoid heat interference and a sufficient heat dissipation area are secured, and then the final placement of ICs is studied.

【Download Documents】 Thermal Design of Semiconductor Components in Electronics

Thermal design has become a new issue in the design of electronic equipment in recent years, as thermal countermeasures have been the focus of attention. Although heat has been an important consideration for some time, the requirements for electronic equipment have changed in recent years, making it necessary to review conventional thermal countermeasures. This handbook describes thermal design based on the assumption that ICs and transistors are basically used in electronic equipment.

    Learn Know-how

    Electrical Circuit Design

    Thermal design

    Switching Noise

    Simulation