Learn Know-how
SPICE Subcircuit Models: MOSFET Example―Part 1
2019.06.20
Points of this article
・There are two types of SPICE models: “device models” and “subcircuit models”.
・Subcircuit models consist of connection information and device models.
・Subcircuit models may be constructed by imparting realistic characteristics to device models that represent ideal characteristics, and may constitute circuits with specific functions or the like.
In the previous article and in the article before that, examples of SPICE device models were explained. In this article and the next, SPICE subcircuit models are explained, using MOSFETs as examples.
SPICE Subcircuit Models (Review)
The basic configurations of device models and subcircuit models were explained in SPICE Model Types, but subcircuit models are somewhat complicated, and so are here briefly reviewed.
Subcircuit models are models of circuits, and such models include circuit connection information, device models, and other information.

In the above example of a subcircuit model that combines an Nch MOSFET and a diode, the circuit connections, a device model of the MOSFET, and a device model of the diode are described. In the “model internal circuit connections”, an instance name is followed by connection terminals and the model name. In this model, the connection of the MOSFET M1 and the diode D1 is described.
Actual Subcircuit Model Example
In the previous explanations, simple models were used to facilitate understanding; here an actual Subcircuit model is used in explanations. The following is a description of the circuit and circuit connections of a subcircuit model for a ROHM Nch MOSFET. In the previous example, the device model for a MOSFET labeled “M1” appeared. The reader will be wondering why we are considering a “MOSFET subcircuit model” when a device model was previously described. This is because a device model is essentially an ideal model, whereas in order to represent the actual MOSFET characteristics, what is often actually used is a subcircuit model, obtained by adding parasitic components, temperature characteristics, and the like to a MOSFET device model that serves as the base. Of course, there are also many subcircuit models of for example circuits in which the components necessary for a power supply IC are connected and the circuit is operated as a power supply, but these would be too complex to use as examples here, and so an example of a MOSFET subcircuit model was selected.

To begin with, examine the descriptions of connections from M1 to R2, and the node numbers in the circuit diagram. The meanings of the descriptions should be immediately understandable.
This subcircuit model is a SPICE model that represents characteristics close to those of an actual MOSFET by adding, to the MOSFET M1 serving as the base model, a feedback capacitance, gate resistance, body diode, and resistance that imparts the temperature characteristic of the on-resistance Ron.
The following is the complete description of the subcircuit model. In addition to the connection information described above, there are descriptions of device models for the MOSFET, diode, and resistances, constituting the subcircuit model. The table lists parameters of each device model.

It should also be noted that in order to create an excellent SPICE model, that is, a SPICE model that represents realistic characteristics, it is necessary to know just what subcircuit models to incorporate. These differ depending on the model source, but it will probably be necessary to confirm the quality of the model, by for example comparing simulation results with actual characteristics.
(Continued to Part 2)
Learn Know-how
Electrical Circuit Design
- Soldering Techniques and Solder Types
- Seven Tools for Soldering
- Seven Techniques for Printed Circuit Board Reworking
-
Basic Alternating Current (AC)
- AC Circuits: Alternating Current, Waveforms, and Formulas
- Complex Numbers in AC Circuit
- Electrical Reactance
- What is Impedance? AC Circuit Analysis and Design
- Impedance Measurement: How to Choose Methods and Improve Accuracy
- Impedance Matching: Why It Matters for Power Transfer and Signal Reflections
- Resonant Circuits: Resonant Frequency and Q Factor
- RLC Circuit: Series and Parallel, Applied circuits
- What is AC Power? Active Power, Reactive Power, Apparent Power
- Power Factor: Calculation and Efficiency Improvement
- What is PFC?
- Boundary Current Mode (BCM) PFC: Examples of Efficiency Improvement Using Diodes
- Continuous Current Mode (CCM) PFC: Examples of Efficiency Improvement Using Diode
- LED Illumination Circuits:Example of Efficiency Improvement and Noise Reduction Using MOSFETs
- PFC Circuits for Air Conditioners:Example of Efficiency Improvement Using MOSFETs and Diodes
-
Basic Direct Current (DC)
- Ohm’s Law: Voltage, Current, and Resistance
- Electric Current and Voltage in DC Circuits
- Kirchhoff’s Circuit Laws
- What Is Mesh Analysis (Mesh Current Method)?
- What Is Nodal Analysis (Nodal Voltage Analysis)?
- Thevenin’s Theorem: DC Circuit Analysis
- Norton’s Theorem: Equivalent Circuit Analysis
- What Is the Superposition Theorem?
- What Is the Δ–Y Transformation (Y–Δ Transformation)?
- Voltage Divider Circuit
- Current Divider and the Current Divider Rule
Thermal design
-
About Thermal Design
- Changes in Engineering Trends and Thermal Design
- A Mutual Understanding of Thermal Design
- Fundamentals of Thermal Resistance and Heat Dissipation: About Thermal Resistance
- Fundamentals of Thermal Resistance and Heat Dissipation: Heat Transmission and Heat Dissipation Paths
- Fundamentals of Thermal Resistance and Heat Dissipation : Thermal Resistance in Conduction
- Fundamentals of Thermal Resistance and Heat Dissipation : Thermal Resistance in Convection
- Fundamentals of Thermal Resistance and Heat Dissipation : Thermal Resistance in Emission
- Thermal Resistance Data: JEDEC Standards, Thermal Resistance Measurement Environments, and Circuit Boards
- Thermal Resistance Data: Actual Data Example
- Thermal Resistance Data: Definitions of Thermal Resistance, Thermal Characterization Parameters
- Thermal Resistance Data: θJA and ΨJT in Estimation of TJ: Part 1
- Thermal Resistance Data: θJA and ΨJT in Estimation of TJ: Part 2
- Surface Temperature Measurements: Methods for Fastening Thermocouples
- Surface Temperature Measurements: Thermocouple Mounting Position
- Surface Temperature Measurements: Treatment of Thermocouple Tips
- Surface Temperature Measurements: Influence of the Thermocouple
- Estimating TJ: Basic Calculation Equations
- Estimating TJ: Calculation Example Using θJA
- Estimating TJ: Calculation Example Using ΨJT
- Estimating TJ: Calculation Example Using Transient Thermal Resistance
- Estimation of Heat Dissipation Area in Surface Mounting and Points to be Noted
- Surface Temperature Measurements: Thermocouple Types
- Summary
- Collection of Important Points Relating to Thermal Design
Switching Noise
- Procedures in Noise Countermeasures
- What is EMC?
-
Dealing with Noise Using Capacitors
- Understanding the Frequency Characteristics of Capacitors, Relative to ESR and ESL
- Measures to Address Noise Using Capacitors
- Effective Use of Decoupling (Bypass) Capacitors Point 1
- Effective Use of Decoupling Capacitors Point 2
- Effective Use of Decoupling Capacitors, Other Matters to be Noted
- Effective Use of Decoupling Capacitors, Summary
-
Dealing with Noise Using Inductors
- Frequency-Impedance Characteristics of Inductors and Determination of Inductor’s Resonance Frequency
- Basic Characteristics of Ferrite Beads and Inductors and Noise Countermeasures Using Them
- Dealing with Noise Using Common Mode Filters
- Points to be Noted: Crosstalk and Noise from GND Lines
- Summary of Dealing with Noise Using Inductors
- Other Noise Countermeasures
- Basics of EMC – Summary
Simulation
- Thermal Simulation of PTC Heaters
- Thermal Simulation of Linear Regulators
-
Foundations of Electronic Circuit Simulation Introduction
- About SPICE
- SPICE Simulators and SPICE Models
- Types of SPICE simulation: DC Analysis, AC Analysis, Transient Analysis
- Types of SPICE simulation: Monte Carlo
- Convergence Properties and Stability of SPICE Simulations
- Types of SPICE Model
- SPICE Device Models: Diode Example–Part 1
- SPICE Device Models: Diode Example–Part 2
- SPICE Subcircuit Models: MOSFET Example―Part 1
- SPICE Subcircuit Models: MOSFET Example―Part 2
- SPICE Subcircuit Models: Models Using Mathematical Expressions
- About Thermal Models
- About Thermal Dynamic Model
- Summary
-
About the ROHM Solution Simulator
- How to Access the ROHM Solution Simulator
- Trying Out the ROHM Solution Simulator (1)
- Trying Out the ROHM Solution Simulator (2)
- Starting a Simulation Circuit in the ROHM Solution Simulator
- ROHM Solution Simulator Toolbar Functions and Basic Operations
- ROHM Solution Simulator: User Interface
- Execution of Simulations
- Method for Displaying Simulation Results
- Simulation Result Display Tool: Wavebox
- Simulation Results Display Tool: Waveform Viewer
- Customization of Simulations
- Exporting Circuit Data to PartQuest™ Explorer
- Purchasing Samples for Evaluation
- Optimization of PFC Circuits
- Optimization of Inverter Circuits
- About Thermal Simulations of DC-DC Converters
- Circuit-Theory-Based Design Simulation